Login

Please login for an individual price calculation.

Forgot Password?
REGISTER AS A COMPANY

We will check whether you already have a customer number with us in order to link your new online account with it.

Register

Contact & Support

Products
Industries and Solutions
Services
Career
Company

Connecting with fieldbus blocks

How data transport through fieldbus blocks works

Connecting with fieldbus blocks

In the second decade after the invention of the PLC, production plants grew rapidly. The system parts and components located there became widely distributed. This led to the next evolutionary step in wiring: the introduction of fieldbuses. A fieldbus is a digital communication network which collects the signals from the individual components through so-called hubs and transports them in the form of telegrams serially to the central PLC. We will show you how the transport works.

Benefits of the fieldbus

Every production machine in an industrial plant has a variety of signals. These signals are transported within a machine (between sensors/actuators/ and the PLC) or across the plant (between different PLCs) via fieldbuses.

The advantage of these fieldbuses is not only in the communication over great distances, but also in the diagnostic function. In addition, signal transmission with a fieldbus requires fewer wires than signal transmission using a junction block.

How fieldbuses differ

There is a variety of different fieldbus blocks:
They differ in their housing material, which is selected depending on the conditions where they will be used. If they are used, for example, in a welding environment, then a block made of fiberglass reinforced plastic is the right choice. Stainless steel is recommended for use in hygienic environments.

They also differ in their connection type, which depends on the bus system being used. Common systems include Profinet, Ethernet/IP or EtherCAT. The fi eldbus block is connected to the controller using a fieldbus cable.

Do you have any questions or suggestions? We are at your disposal.

For all questions concerning commercial topics such as quotations, orders, delivery times, our inside sales department will be happy to support you.


Balluff GmbH

Schurwaldstraße 9
73765 Neuhausen a.d.F.